HALO Fire Safe Solutions | Fire Rated Recessed Lighting | Cooper Lighting Solutions
Apartment mailroom with HALO HLBFR fire rated canless downlights in matte black
Fire Safe Solutions

Code compliant.
Easy to install.

HALO fire rated canless downlights and new construction housings can prevent the passage of flames and toxic gases through the ceiling for up to two hours in accordance with UL 263. Canless downlights mount directly to the ceiling, with no need to build drywall boxes or use fire rated covers.

UP TO2HRS

Fire rated up to 2 hrs. Canless downlights and new construction housings are tested to UL 263. The JB4FR2 meets up to two hours per International Building Code Section 714.

UL 263International Building Code, Section 714
HLBFR in matte black · apartment mailroom

We have you covered

HALO has a full line of fire rated downlights and housings. Safe, tested and trustworthy.

HALO JB4FR2 hybrid junction box housing with Pass-N-Thru hanger bars
STANDARD OR FIRE RATED CEILINGS
JB4 4″ Hybrid Junction Box Housing
JB4FR2 · round 4″ · new construction

For use with any HALO 4-inch LED trim or any sized HALO surface mount downlight, with up to 2-hour protection per International Building Code Section 714. Pass-N-Thru™ hanger bars allow toolless shortening in tight spaces (7″ to 24″).

  • IBC 714 · up to 2 hrs
  • AIR-TITE
  • Wet rated
  • All-Nail!™
  • Pass-N-Thru™

AIR-TITE and wet location suitability are based on the installed LED trim or surface mount fixture.

HALO RLFR fire rated recessed baffle canless downlight
Canless · remodel or new construction
RLFR canless downlights

Fire rated recessed baffle canless downlights in 4 and 6 inch. Canless downlighting mounts directly to the ceiling for easy remodeling. For new construction, add a HALO Canless Mounting Frame during rough-in to reserve the location. True protection: ceramic fiber insulation withstands temperatures up to 1850° for up to 2 hours.

  • UL 263 · up to 2 hrs
  • 5 color temperatures
  • No housing required
HALO HLBFR fire rated slim low-glare canless downlight
Canless · remodel or new construction · slim, low-glare
HLBFR canless downlights

Fire rated slim canless downlights in 4 and 6 inch, with a die-cast trim and low-glare prismatic lens. Spring-loaded arms hold the fixture directly to the fire rated ceiling for a secure, AIR-TITE fit. 5-Color Field-SeleCCTable™: use the switch on the back of the fixture to choose 1 of 5 color temperatures, from warm white (2700K) to daylight (5000K).

  • UL 263 · up to 2 hrs
  • 5 color temperatures
  • No housing required
HALO Fire Rated New Construction Housing with 2-hour fire rated label
New construction housings
Fire Rated New Construction Housings
H350FR2ICAT 3″ · H450FR2ICATD010 4″ · H550FR2ICATD010 5″ · H750FR2ICATD010 6″

Double walled new construction housings filled with fire rated material, available in 3, 4, 5 and 6-inch apertures. Use with HALO LED integrated trims. No need to build drywall boxes or use fire rated covers.

  • UL 263 · up to 2 hrs
  • AIR-TITE
  • Wet rated

UL 263 RLFR and HLBFR canless downlights and the Fire Rated New Construction Housings are tested to UL 263 and can prevent the passage of flames and toxic gases for up to two hours.

IBC 714 The JB4FR2 junction box housing is suitable for ceilings that require up to two hours of protection when installed per International Building Code Section 714. AIR-TITE and wet location suitability depend on the installed trim or fixture.

See it in the space

Fire rated ceilings don't have to look like it. HALO Fire Safe Solutions mount flush to the ceiling in the kitchens, entries and common areas where the rating matters. Tap the markers, or tap a photo to look closer.

Apartment kitchen and entry lit with HALO HLBFR fire rated canless downlights
Apartment kitchen and entry. HALO HLBFR fire rated canless, with HALO SMX surface mount in the entry.
Apartment mailroom with HALO HLBFR fire rated canless downlights in matte black
Apartment mailroom. HLBFR in matte black against a dark ceiling.

Two finishes, both fire rated

Matte white for bright ceilings, matte black for dark ones. RLFR and HLBFR come in both, in 4″ and 6″.

Save time and money

No need to build drywall boxes or use fire rated covers. A factory-tested fire rated solution eliminates the need for separate fire boxes, which saves time and labor.

UNIT ABOVE UL 263 CEILING PLENUM UNIT BELOW FIRE RATED CEILING SPRING ARMS
Per fixtureStandard downlight in a fire rated ceilingHALO RLFR or HLBFR canless
PartsFixture, plus a drywall box or fire rated coverFixture only. No housing required.
InstallationBuild the box or fit the cover around the fixtureMounts directly to the ceiling
Time and laborExtra work at every fixtureSaved, with no separate fire box
Fire ratingRestored by the box or coverUp to 2 hours in accordance with UL 263

Keeping existing fixtures? Where standard fixtures stay in a fire rated ceiling, codes often call for enclosures to restore the ceiling's fire resistance. HALO canless fits fire rated ceilings between ½″ and 2″ thick.

One hour or two?

The project drawings set the rating. HALO Fire Safe Solutions are suitable for ceilings that require up to two hours of protection. Answer three questions to see which HALO products fit.

Suitable for multi-family and mixed use

Safe, tested and trustworthy for apartment buildings, townhomes and condos, and for commercial applications where safety is paramount. Pick a building type to see where the rating shows up and what fits.

Rules vary by jurisdiction, so confirm the governing code, such as the IRC or IBC, with the local authority.

For specifiers and designers, agents and distributors, contractors and installers, facility managers and municipalities.

Common questions

Straight answers for specifiers, contractors and facility teams.

Do recessed lights need to be fire rated?
It depends on the ceiling. Where a ceiling is fire rated, building codes often require fire rated downlights or enclosures to restore its fire resistance. That is common in multi-family buildings and townhomes where ceilings or floors separate dwelling units, beneath attached garages or bonus rooms, and in two-story homes with finished basements or attics where penetrations connect one habitable level to another. Rules vary, so check the governing code, such as the IRC or IBC, with the local authority.
How do I know whether my ceiling is rated?
Check the project drawings and the governing code, such as the IRC or IBC. Jurisdictions may adopt stricter standards, so confirm requirements with the local authority rather than assuming.
Are canless lights fire rated?
Only models tested and listed for it. HALO RLFR and HLBFR canless downlights can prevent the passage of flames and toxic gases for up to two hours in accordance with UL 263, and they mount directly to the ceiling with no housing required.
What is the difference between a fire rated fixture and a fire box?
Both restore the ceiling's fire resistance. A fire box, such as a drywall box or fire rated cover, is built or fitted around a standard fixture. A fire rated fixture is factory tested to do the job on its own, which eliminates the need for a separate fire box and saves time and labor.
Do I still need an enclosure if the fixture is rated?
No. With HALO Fire Safe Solutions there is no need to build drywall boxes or use fire rated covers. Install within each product's listed conditions. HALO canless, for example, fits fire rated ceilings between ½″ and 2″ thick.
Can I add fire rating to a light I already installed?
Codes often require fire rated downlights or enclosures to restore a rated ceiling's fire resistance, so an existing standard fixture usually means adding an enclosure or replacing the light. In a finished ceiling, HALO RLFR and HLBFR canless downlights mount directly to the ceiling for easy remodeling.
One hour or two?
The project drawings and the governing code set the required rating. RLFR and HLBFR canless downlights and the new construction housings were tested for two hours in accordance with UL 263, and the JB4 junction box housing provides up to two hours of protection per International Building Code Section 714. A two hour rating generally implies compliance with a one hour rating, but some building codes or clients may require explicit documentation for the one hour standard, and certain applications or jurisdictions may require products tested and certified specifically for the intended fire-resistance duration. Always check local building codes, fire safety regulations and project requirements to ensure compliance.
What should I document for inspection?
Verify each fixture's listing and test standard, such as UL 263 or ASTM E119, and document it for inspectors. Even a quick photo of the product label can save a costly return trip.

We have you covered

HALO Fire Safe Solutions from Cooper Lighting Solutions. Fire rated downlights and housings that are code compliant and easy to install.