Oil & Gas Lighting Turnaround Planning Guide | Cooper Lighting Solutions
Oil & Gas Turnaround Guide

WHY TIMING DECIDES THE OUTCOME

A turnaround is the one window where classified-area lighting work gets easy.

Once the unit is down, permits are in place and crews are already on site, classified-area fixtures can be replaced without a separate shutdown. Miss that window and the next chance is a year and a permit away. This guide maps the lighting decisions to the turnaround calendar so the work lands inside the window instead of after it.

WHAT THE GUIDE COVERS

Pre-window audit through post-window validation.

A step-by-step path across the full turnaround timeline.

  • 12 to 18 months out. Scope the classified-area fixtures, confirm area classifications, and build the lighting line items into the turnaround plan before budgets lock.
  • In-window execution. Stage certified fixtures and retrofit adapters so the install runs without a fixture-type surprise mid-outage.
  • Post-window validation. Confirm the layout meets target levels and document the work for close-out.

BUILT ON THE FULL PORTFOLIO

Certified for the areas that matter most.

The guide is grounded in the Cooper Lighting Solutions oil and gas portfolio, with Nemalux carrying the Class I Division 2 and IP66/67 ratings classified areas require, plus retrofit adapters built for turnaround and shutdown scenarios.

GET THE GUIDE

Download the Turnaround Planning Guide

Tell us where you sit on the project and we will deliver the guide right away. If your role flags a live project, an application engineer can follow up with portfolio and photometric support.

By submitting you agree to receive emails from Cooper Lighting Solutions in accordance with the Cooper Lighting Solutions Privacy Policy.

" "